(0)| 9/12/2009 6:38 AM | |
|
Joined: 12/18/2007 Last visit: 9/2/2025 Posts: 24 Rating:
|
Dear sirs, I am using CU320 and CF card V02.06.01.00. My Scout Software is Product: SCOUT,Release: V4.1.2.4. SSP SINAMICS V2.6 SP1 Version: V2.61.0.0,Release: V02.60.35.00_04.03.00.00 Now problem is,When I downloadtheconfiguration from PG,first time it is loaded 100% to CU,without anyproblem. Again download the same configuration to same CU it is load upto 74%. After long time the following error is displayed. I herewith attached the error details.Same time the CU RDY LED colour is Orange. please give me the solution about this Problem. Thanks & Regards, AttachmentError detailes.pdf (506 Downloads) |
Follow us on