4/28/2022 4:22 AM | |
Joined: 10/4/2017 Last visit: 1/19/2023 Posts: 2 Rating: (0) |
Hello all! I have been struggling with mi logo v8.3, I can connect correctly to the router, I can register correctly the "thing" , I can deploy correctly to the cloud with logo web editor, but when I try to set a bit from the web page it does not work. I set this bit from a kpt400 I have connected to the logo and I can see the change in the device's shadow in aws. It is very frustrating since I have double checked connections, & the program in the logo, permissions in aws and all seems to be ok but I can communicate to the logo from the webpage created in LWE... permissions used in aws are: • AWSIoTFullAccess • AdministratorAccess-AWSElasticBeanstalk • AWSElasticBeanstalkReadOnly I have checked a video I found here & the only difference I noticed is that they are using tomcat platform version 4.1.4 & I'm using 4.2.13 I can not change it since aws uses it by default & tried to change but does not allow it. AttachmentBit testing.pptx (447 Downloads) |
Last edited by: anty_8506@hotmail.com at: 04/28/2022 04:50:35Last edited by: anty_8506@hotmail.com at: 04/28/2022 23:48:04 |
|
Follow us on