2/19/2021 11:52 AM | |
Joined: 7/5/2018 Last visit: 2/22/2021 Posts: 1 Rating: (0) |
I have a problem with DIGSI 5 V8.40 installation. The story is I ran the setup.exe, follow the instructions, it was all fine, until at the end I decided to click Restart Later. After a machine restart some time later, it does not allow the installation to continue. When I ran the setup.exe again, it kept telling me that the machine has not restarted. Now I am stuck in this and there is no way to proceed further or rollback. I then installed V8.00 instead, hoping this can get resolved later. AttachmentDIGSI_V8.40_SetupBundle.txt (704 Downloads) |
2/19/2021 12:28 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054) |
hi hy.yam, maybe this FAQ helps: How do you disable the message "Please reboot before installing any more programs"?regards, |
FCK WAR! |
|
This contribution was helpful to1 thankful Users |
2/7/2022 9:52 PM | |
Joined: 2/7/2022 Last visit: 2/7/2022 Posts: 1 Rating: (0) |
I'm having the same problem. Need to restart the computer to continue. Does anyone have a solution? |
3/7/2024 1:44 PM | |
Joined: 8/21/2014 Last visit: 9/27/2024 Posts: 1024 Rating: (14) |
New question published by Edmilson de Andrade is split to a separate thread with the subject Issue with DIGSI 5 v9.7 installation. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on