5/8/2024 8:37 AM | |
Joined: 4/16/2024 Last visit: 5/8/2024 Posts: 1 Rating: (0) |
Hi everyone! I am working with ABB ACS 550 drive and using Profibus adaptor RPBA with PPO 4. Now i need to change the drive to ABB ACS 880 and using FPBA 0-DP-V1 which having a software version 3,20. which PPO type i need to use to make it work with PLC CODE. GSD file which i have showing different PPO-04 För example PPO-04, 0PW + 6PZD PPO-04, 0PKW +(2+2+2)PZD PPO-04, 0PKW + NOcONS.6PZD In the RPBA there is only PPO1,02,03,04 but there is many more so question is which one should i use to get same io size and other functionalitys? Thanks in advance. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/08/2024 12:54:49New subject after splitting |
|
Follow us on