6/27/2024 10:53 AM | |
Joined: 10/18/2019 Last visit: 7/29/2024 Posts: 1 Rating: (0) |
Greetings all, I have this same issue in WinCC professional v19 upd2 (TIA portal) and there is no "Allow drag in Runtime" or similar property on an I/O field. Also I think because of this we can only input a value on one of the edges of the I/O field once a tag is linked to it. If a tag is not linked to it you can click anywhere on the field to input the value and also there is no drag feature on it (or hand icon). Any help would be appreciated. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/28/2024 06:49:27New subject after splitting. Quote inserted. |
|
Follow us on