7/12/2024 11:27 AM | |
Joined: 6/23/2013 Last visit: 8/1/2024 Posts: 62 Rating: (6) |
The new 3.20 version, which will be released shortly (the documents from it are already available), has more options too choose from to install. The UI can be installed as an own option, so it is not needed to install the DesktopUI anymore. Perhaps also take a look at the product packaging documentation, it seems that the MSI are also available. But perhaps the best course is to make an official request to be able to set the installation path for the DesktopUI. |
WinCC OA expert |
|
Follow us on