7/25/2024 2:27 PM | |
Joined: 4/30/2024 Last visit: 10/11/2024 Posts: 2 Rating: (0) |
Hello Everyone, We have a Simoreg that is going to be replaced by a Sinamics DCM. We'll keep profibus DP to communicate with the PLC. The Simoreg isn't using any telegram as you can see in the attachment. I intend to do the same for the Sinamics DCM. So I was thinking about to use the free telegrams with the same numbers of input/output words. Are free telegrams the correct way to do that? Could you give-me any suggestions? I just read the DCM manual but it couldn't help-me. Best Regards. AttachmentSimoreg.docx (252 Downloads) |
9/30/2024 11:07 AM | |
Joined: 4/30/2024 Last visit: 10/11/2024 Posts: 2 Rating: (0) |
Hello, I just used the free telegrams with the same number of IO data. It worked fine. Case closed! Best regards |
Follow us on