7/29/2024 4:42 PM | |
Joined: 8/23/2022 Last visit: 8/8/2024 Posts: 5 Rating: (0) |
Hi, Is it possible to read a HMI SD card on a Somatic Field PG M6 or any kind of PC with a SD reader ? Kind regards, |
7/30/2024 7:31 AM | |
Joined: 5/6/2022 Last visit: 9/27/2024 Posts: 455 Rating: (90) |
Hi AutoGen_5950671, In principle you should have no problem reading SD cards from a PC with a reader. The only thing you should be careful about is that if you are going to format the SD card from the PC, you should not delete the hidden files. Otherwise, there should be no problem. Best regards!
|
If this Information really helps, you could use the Rate function |
|
Follow us on