9/25/2024 7:45 AM | |
Joined: 2/5/2023 Last visit: 10/28/2024 Posts: 16 Rating: (0) |
Hi I think you say TIA Portal and use Device proxy. I have question about Wincc Professional Eng v17/19 (TIA portal) and S7-400H. the program composed in Simatic manager v7.5 and I want to use this program and connect it to new SCADA according to this link . this is compatible to use them (Wincc Professional (TIA portal) and S7-400H) together? Sincerely ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 09/25/2024 07:50:52New subject after splitting Last edited by: student20 at: 09/25/2024 09:29:11 |
|
9/29/2024 6:43 AM | |
Joined: 2/5/2023 Last visit: 10/28/2024 Posts: 16 Rating: (0) |
I’ve downloaded sample S7-400H project (Realization of a Fault-Tolerant Tunnel Lighting System With S7-400H) from this link and the program wrote in Step7 v5.5. I import it to Device proxy in TIA Portal v17 and then add Wincc RT Advanced/Professional. The schematic PDF file is attached. AttachmentS7-400H.pdf (129 Downloads) |
Last edited by: Moderator_Lan at: 09/30/2024 09:14:30link optimized |
|
9/29/2024 1:55 PM | |
Joined: 2/5/2023 Last visit: 10/28/2024 Posts: 16 Rating: (0) |
To call VB script, I must use “event” to monitor changing value of “trigger_PLC1” tag (step.7 in this link), but I can not use “event” in Wincc RT Professional!! |
Follow us on