8/1/2006 8:03 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (318)
|
[quote user="Survive"]I bought a CP 5512 but I didn't buy the connectors. So, what are the correct connectors for the both end points of the cable? Please, tell meboth Siemens code. One more thing, what is the difference between "Profibus fastconnect busconnector" and "Profibus standard connector" ? I saw in the manual the code 6GK1 500-0FC00 (180') to connect withCP 5512, but do I need two connectors with this code ?? Hi Survive, Wenn you don't need to do special things you can use a Profibus Cable with normal Profibus DP Fastconnect connectors. A Profibus FC connector is very quick to turn on a cable, there is a Profibus Fast Connect Stripping Tool where with even I can make the connector in 20....30 seconds on a Profibus Cable without any trouble. [:blush:] A standard cable works with screws and there you have to strip the wiring by your self.... it is a crime to do that when you have used FC tool and cable. [:mad:] A little booklet where this is even better described than I can do that: Instructions for stripping the insulation from SIMATIC NET PROFIBUS Fast Connect cables So you may try it for your CP 5512 to make a cable with those connectors and the stripping tool. [;)] The connectors are in differend types, with and without PG on top of it. (90, 135 and 180 degrees). |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
8/3/2006 7:27 AM | |
Posts: 2348 Rating: (264) |
It's not recommended - at PROFIBUS connector there is terminal resistor, which is used for creating net configuration. |
Follow us on