8/6/2006 10:45 AM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (318)
|
[quote user="FIE-Auto"]It is a CP 341 with RS232 interface. Now you mean that I should connect the CP to PC with a RS232 cable directly? And can I do it through Modem? I mean connect the CP to Modem and PC to Modem and then dial the CP from PC? Hi, What do you want to make, communication directly with a PC? Then you could make directly contact with the RS232 port of the PC with a crosscable [:o] The only thing is that you have to choose for a protocol ASCII or something like that. And then write on the CPU-side a programm or look in the examples that are installed when you install the PtP package. [8)] Also Modbus Master or Slave is possible, but then you need a Modbus Master or Slave package on the CP341 and on the PC. Good Luck with your experiment. [;)] |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on