8/16/2011 11:04 AM | |
Joined: 12/27/2006 Last visit: 8/18/2024 Posts: 1197 Rating: (113) |
Go to File > Properties or with the key's Alt+Enter Tab parameter, There you can adjust the settings of the AQ Thats what you want? Or do you mean something i have made in this programm: Setteing the startvaluwe in B002 - V1 AttachmentAnaloge_Start.zip (271 Downloads) |
Last edited by: Toeternietoe at: 8/16/2011 11:20 AM |
|
8/16/2011 4:19 PM | |
Posts: 2 Rating: (0) |
Dear Toeternietoe, thank you for your reply. I am managing Digital Outputs (relay outputs) and not analogue. I am attaching a very short program (3 lines) in which after activating and deactivating I1, Q1 is activated, even if I reset the program from tue plug icon, and even if I quit simulation mode back to edit mode and to simulation again. If I want to restart the program I need to colose the file and re-open it... AttachmentRetencion1.zip (294 Downloads) |
Follow us on