5/15/2007 2:10 PM | |
Posts: 86 Rating: (2) |
Late, Do you mean it will work on S7-414H CPU? I am using this for another project, don't have the system ready yet, so not able to test it. Thanks, Techy |
5/15/2007 5:38 PM | |
Joined: 12/5/2005 Last visit: 5/22/2024 Posts: 239 Rating: (9)
|
Hi Techy, I believe that it works, althoughI never tested the force on analog values. But to work in this case, you can't access the analog values by direct image peripheral (PIW and PQW), you have access the values by image peripheral (IWand QW) See the post: http://support.automation.siemens.com/WW/view/en/18325417 |
Márcio Santos |
|
This contribution was helpful to1 thankful Users |
5/30/2007 12:33 PM | |
Posts: 86 Rating: (2) |
Marcio, Thanks for the information. I will try it out as soon as I get access to the hardware. Thanks, Techy |
Follow us on