11/12/2005 12:56 PM | |
Posts: 102 Rating: (9) |
Hi I want to configure a Redundant industrial network, with 12 PLC S7-400F, 4 PLC S7-400FH , 1 WinCC Server with 2 network and 2 WinCC client. I have read the following documents: CommunicationManual_e.pdf S7-400H_e.pdf mn_osm-esm_76.pdf I configured the network like the attachment file in two ways. Please tell me if they are correct.and witch one is better? Another question is which softwares do I need to managment this network? Thanks Mehrnoosh Attachmentnetwork1-2.zip (580 Downloads) |
11/14/2005 10:53 AM | |
Posts: 102 Rating: (9) |
Dear Mohammad[:)] Thanks for your help. So both configurations are correct but the seconde one is better. Best Regards Mehrnoosh |
Follow us on