5/9/2017 6:55 AM | |
Posts: 20 Rating: (2) |
Hello, I am doing a project using IOT2020 to control the speed of a motor using PWM technique .I just want know that is there any controlling action that can be done using the IBM Bluemix IoT Platform .basically i need to send data from the platform to the iot to control the motor. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/9/2017 1:22:22 PMNew subject after splitting |
|
5/15/2017 8:35 PM | |
Posts: 9 Rating: (1) |
Try using mraa Pwm class. It automatically outputs the PWM by using its write function to specify an analog value: https://iotdk.intel.com/docs/master/mraa/classmraa_1_1_pwm.html |
Last edited by: bamsbamx at: 5/15/2017 8:36:18 PM |
|
2/26/2018 7:53 PM | |
Posts: 4 Rating: (0) |
Please, do you have an example of sending data from IBMIOT node to the gateway ? |
Follow us on