7/14/2020 1:42 PM | |
Posts: 8 Rating: (8)
|
The SIMATIC HMI Unified Comfort Panels are part of the newly developed SIMATIC WinCC Unified System. In addition to numerous new functions offered by the new hardware and software, the SIMATIC HMI Unified Comfort Panel can also be used as an edge device. This additional option allows additional functions and customer-specific requirements to be implemented that are not covered by the standard scope of the SIMATIC WinCC Unified System. Where can I find the appropriate information about Edge on the Unified Comfort Panel? Unified Comfort Panels for Industrial Edge manual: https://support.industry.siemens.com/cs/ww/en/view/109773259 Industrial Edge Publisher manual: https://support.industry.siemens.com/cs/de/en/view/109778824 Industrial Edge Publisher download: https://support.industry.siemens.com/cs/de/en/view/109778875 Industrial Edge in connection with Simatic HMI Unified Comfort Panel application example: https://support.industry.siemens.com/cs/ww/en/view/109778780 |
Last edited by: Industrial Edge at: 07/20/2020 20:02:25 |
|
This contribution was helpful to3 thankful Users |
Follow us on