11/14/2022 9:50 PM | |
Joined: 5/29/2014 Last visit: 5/16/2024 Posts: 9 Rating:
|
Hello everyone, I have a few questions regarding the migration from Step 7 v5.x to TIA. [snip] In the current program the block below is used once, which is only working on the old 314IFM CPU. SFB39 Position (Integrated Function, CPU 314 IFM)
Please note that we don't have much information/comment about the program and the functioning. The manufacturer of this device went bankrupt 14 years ago. At the moment we only have a download of the program, supplemented with symbolic names from the electrical diagrams. In attachment I’ve added an image of the network with the SFB39 and associated DB39 block. Any info is welcome to point me in the right direction. Thanks in advance. Kind regards, ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/15/2022 07:32:13New subject after splitting. Division of questions into separate topics. |
|
Follow us on