10/2/2023 3:49 PM | |
Joined: 10/25/2016 Last visit: 5/30/2024 Posts: 3 Rating:
|
Hi! I am working on a project were we will be replacing an 300 CPU with a 1500 CPU and we are working on migrating / converting code. There is a integral block used to handle analog signals, write/read to Cont_C regulator as well as read/write to WinCC with Static variables and OS messages. I have removed segments of the code that was related to OS messages, we will be instead using Program Alarms. It would be GREATLY appreciated if we could get some help with converting the STL code to something easily understandable (not used to STL I guess, always worked in SCL + FDB). The code is the following: A rather large amount of code so do not expect someone to have the time/effort to help us but thought it would be worth a shot Kind regards, Olle Z AttachmentCode.txt (275 Downloads) |
Last edited by: AutoGen_8431264 at: 10/03/2023 10:53:52Last edited by: Jen_Moderator at: 10/12/2023 13:58:31Code added as .txt file. |
|
10/3/2023 10:14 AM | |
Joined: 6/20/2017 Last visit: 8/17/2024 Posts: 396 Rating:
|
Thaks. |
Gustavo Antonio Banchetti Brucatori. |
|
Follow us on