12/12/2023 12:15 PM | |
Joined: 2/17/2023 Last visit: 5/8/2024 Posts: 1 Rating:
|
hey guys! I'm having difficulty configuring the iot2050 advanced FS:05. I downloaded the example image v1.1.1, but then I saw that for FS:05 it would have to be v1.3.1, I'm waiting for SIEMENS to release the download. I also tried IOT2050_IndustrialOS_Service_Stick_V3.2.3.zip (7.8 GB), I recorded it on the uSD using the win32disk imager and inserted it into the iotried remote access via ethernet cable using the default IP 192.168.200.1 but it is not working, I also tried using DP and keyboard but nothing appears on the monitor. I am following the steps for Industrial OS V3.2.2 on SIMATIC IOT2050 - Getting Started and Setting up the IOT2050 with Example Image but none worked. what could be happening? ------------------------------------------------------------------------------------------ . |
Last edited by: The Helping Hand at: 12/12/2023 13:14:44New subject after splitting and Text formatting optimized |
|
Follow us on