3/27/2024 4:30 PM | |
Joined: 12/16/2022 Last visit: 7/15/2024 Posts: 5 Rating:
|
It appears that S7-GRAPH elements aren't version tracked; only STL/SCL stuff, correct? [snip] ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/28/2024 09:29:09New subject after splitting. Division of questions into separate topics. |
|
3/28/2024 9:30 AM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8176 Rating:
|
New question published by aanse is split to a separate thread with the subject Does anyone have experience with other Git-like version control systems, such as Copia?. Best regards |
My Forum is the place to personalize your profile, |
|
3/28/2024 4:54 PM | |
Joined: 12/14/2022 Last visit: 7/9/2024 Posts: 63 Rating:
|
If you are talking about the TIA Version Control Interface (VCI), "You can manage the following object types with an external version control program: > Organization blocks (OB) > Function blocks (FB) > Functions (FC) > Data blocks (DB) > PLC data types > PLC tag tables You can also use these as failsafe objects if no password was set for them or if you know the password. The following objects, however, cannot be synchronized with an external version control program: > CEM blocks > Blocks with know-how protection > Library types The supported objects cannot be edited with the workspace editor. They can only be edited in the relevant editors such as the program editor. Changes to the above object types in the project are automatically applied in the workspace editor. The project area therefore always reflects the latest version of the project. You have the option of configuring an external comparison program. You can use it in the workspace editor afterwards to determine the differences between an object in the project and a workspace file connected to it." |
Last edited by: Igor_Coraine_ at: 03/28/2024 16:55:43Last edited by: Jen_Moderator at: 03/30/2024 08:02:26Text formatting optimized. igorcoraine.github.io |
|
Follow us on