9/7/2011 3:44 PM | |
Posts: 8 Rating: (0) |
Thank you for the reply. Unfortunately at this time I do not posess the AK 1703 ACP Toolbox configuration files. I am working on a small qt&c++ project to develop a HMI application for presentationpurposes.This application has to receive data from the AK1703. All i have are some log files generated with TMW Protocol Test Harness while conecting it to the AK1703.I attach them so you can see. It is very sad to hear that SIEMENSIEC60870-104 implementations are not standard compliant. I am not very familiar with the Toolbox II configuration suite. Could someone send me some screen shot of witch settings can i modify ...or play with to see if anything changes? AttachmentLOGS.zip (361 Downloads) |
Follow us on