6/9/2018 11:21 AM | |
Joined: 1/24/2009 Last visit: 3/29/2024 Posts: 85 Rating: (7) |
Hello, i have used in S71500 an FB written in STL. Now i want to use it in S71200, so i have to translate it to SCL. Is there any easy way ? Could someone help with a conversion tool maybe ? Attached my code AttachmentSTL code.docx (1132 Downloads) |
6/9/2018 2:21 PM | |
Joined: 11/29/2011 Last visit: 9/26/2024 Posts: 1359 Rating: (232) |
Hi, There is no tool like this I do not think. See the same discussion here: How to convert STL to SCL after uploading STL to PG from PLC. Maybe you could consider rewriting the code in SCL. It is not a big code and what you will find in SCL, that the code is even simpler. If you specific question about how to reimplement certain code elements please come and ask. |
Last edited by: MicroMan at: 6/9/2018 2:22:30 PM- What you read here, please check with manuals and your requirements. |
|
This contribution was helpful to3 thankful Users |
6/9/2018 10:39 PM | |
Posts: 2826 Rating: (685) |
Hello.
Today is your birthday! ;-) It is up to you to test it and see if it is correct. I suggest loading the FB to run along with the original STL one and see if the SCL version follows the STL version. AttachmentRRI_FB_LAG1ST.zip (1093 Downloads) |
This contribution was helpful to3 thankful Users |
Follow us on