3/17/2011 8:20 AM | |
Posts: 17 Rating: (0) |
Thank you for your response. What system are you using? I mean, are you using S7-Analyzer with PROFINET as protocol? DoesPROFINETalso capableof achieving 5ms sampling rate? |
3/18/2011 1:22 AM | |
Joined: 10/7/2005 Last visit: 9/30/2024 Posts: 3023 Rating: (1054) |
Hello Aevat I need to stick with my previous advise which is: ibaPDA S7 Analyser Aquisition speed depends on a number of factors (e.g. number of signals to be aquired, network traffic, CPU type and communciation load etc.), but expect to get update rates of typically 10ms to 30 ms with modern PN CPU's. This is based on experience (I always haveibaPDA-S7-Analyser with me when doingcommissioning or troubleshooting taks on S7 PLC's). The offical iba advise can be found in the ibaPDA-S7-Analyser manual, note that the test was done with a 416 CPU and external CP443-1 Ethernet card (a PN port of a CPU won't be slower though) and attached is the extract from the manual. My advise: Once you start using ibaPDA-S7-Analyser you will wonder how you ever did any commissioning or troubleshooting taks on S7 PLC's without it (for the record, I do work for ibaOceania so this advise may be perceived to be biased. Take my word for it though that I'dgive the same advise ifI wouldn't be part of the iba team). I hope this helps |
Cheers |
|
3/18/2011 4:14 AM | |
Joined: 10/7/2005 Last visit: 9/30/2024 Posts: 3023 Rating: (1054) |
Hello Aevat please get in touch with ibaAsia (e-mail: iba@iba-asia.com) and they'll advise on the best course of action. |
Cheers |
|
This contribution was helpful to1 thankful Users |
6/1/2016 1:06 PM | |
Posts: 26 Rating: (0) |
Dear sir, Is there any way to communicate IbaPda on Ethernet IP with RsLogix 5000 ( Allen Bradley ) plc, this plc is having Ethernet IP card installed on slot no.7 what are the steps to be followed during communication. i have attached pdf file with warm regrads Deepak
AttachmentHow to communicate Rslogix5000 controller_with IbaPda.pdf (524 Downloads) |
6/1/2016 3:22 PM | |
Joined: 10/7/2005 Last visit: 9/30/2024 Posts: 3023 Rating: (1054) |
Hello Deepak it is absolutely possible to acquire Ethernet/IP based data from a Rockwell PLC. This does though require PLC configuration (setup of an EIP output module and data marshaling to it outputs) as well as the corresponding ibaPDA configuration. You would have received the ibaPDA-Interface-Ethernet/IP manual when you bought the software and it contains detailed examples on what to do. If you've lost the manual please get in touch with your nearest iba office and they'll look after you. |
Cheers |
|
8/5/2019 11:46 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by HSCDP is split to a separate thread with the subject Data Aquisition Using ibaPDA - How many signals recommend to be archived in a Plant with 6K I/Os?. Best regards |
8/5/2019 11:48 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by HSCDP is split to a separate thread with the subject What is the justification for using the unlimited license of ibaPDA?. Best regards |
Follow us on