10/9/2023 5:19 PM | |
Joined: 10/2/2023 Last visit: 11/8/2023 Posts: 20 Rating: (0) |
Or do you just want to specify the setpoints values only via the web server? YES this is what I want. |
10/9/2023 5:40 PM | |
Joined: 10/2/2023 Last visit: 11/8/2023 Posts: 20 Rating: (0) |
Than you very much!! |
10/9/2023 6:31 PM | |
Joined: 12/18/2014 Last visit: 9/28/2024 Posts: 33846 Rating: (4208)
|
In attachment the program and the project. I see a problem with the sliders by using a handy. The sliders are very small and so it is very complicated to find the right setpoint. I have make some changes in your LOGO! program. - You don't have make the same settings in the analog amplifier and then also in the following threshold triggers. In the threshold triggers must you set the gain and offset as the default values. - I have deleted the NOT blocks, you don't need them. You can better negate the input pin of the block. - I have added a second page in the diagram for better reading the diagram. AttachmentPellet burner V2.zip (597 Downloads) |
Follow us on