2/28/2021 3:16 PM | |
Joined: 9/27/2006 Last visit: 9/28/2024 Posts: 12283 Rating: (2685) |
Hello M.Amgd; The only PC Adapter model that Siemens certifies as compatible with Windows 10 (32- or 64-bit) is the PC Adapter USB A2 (MLFB: 6GK1571-0BA00-0AA0). Is this the model you want to install with Step 7 v5.6? In that case, look at the Operating Instructions manual for this adapter. The screenshot below includes an extract of the relevant details for your question. https://support.industry.siemens.com/cs/ww/en/view/68849363 If you do not have access to the CD containing the driver, you might have a problem. It comes with the new purchase of the adapter, and there are no downloads of this driver from Siemens Support. There are some sites that offer this download, but they are not from Siemens, so be very careful if you decide to download these files. Hope this helps, Daniel Chartier |
Follow us on