6/21/2024 7:43 PM | |
Joined: 1/10/2023 Last visit: 9/24/2024 Posts: 1 Rating: (0) |
Hello! Product is incompatible with an already installed product from a different SIMATIC product series: all versions of WinCC V6.x/V7.x Please remove the "WinCC" instance of the SQL Server because it still exists in an incompatible version for TIA Portal V17 WinCC Prof Ed after a de-installation of "WinCC Professional" or "WinCC Runtime Professional". Can you help me what to do?
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/24/2024 08:26:22New subject after splitting |
|
6/27/2024 8:42 AM | |
Joined: 8/3/2009 Last visit: 9/27/2024 Posts: 13803 Rating: (1741)
|
Hello AutoGen_2226495 With V17 there are two different Installation DVDs: https://support.industry.siemens.com/cs/de/en/view/109784440 One with WinCC Professinal and one with Unified. If you have already installed a WinCC Professional or WinCC V7/8 on your System then you can only work with the WinCCUnified installation medium. Here you should be able to install WinCC Comfort/Advanced parallel to your WinCC V7. But not WinCC Prof or Unified this is not released on the same system. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on