4/20/2023 6:57 AM | |
Joined: 4/15/2022 Last visit: 7/31/2024 Posts: 28 Rating: (0) |
Hi! I`m learning SCL from the manual, and I tried to simulate the project they offer in the manual. But when I compiled it returns some errors. I declared in the symbol table as required. I find that in the SQUARE block / function they declared an INT named ”value” and below in the formula is used as ”val”. How is possible to add an example in the manual without compiling before? Or I am missing something. I attached the project. Thx! AttachmentScl.zip (667 Downloads) |
4/23/2023 9:43 AM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (820) |
Hello,
eeeeehm sry maybe I'm blind but where do you see that val variable in formula???? |
With best regards... |
|
4/24/2023 9:25 AM | |
Joined: 4/15/2022 Last visit: 7/31/2024 Posts: 28 Rating: (0) |
Here is! What version of the manual do you have? check the latest one |
4/25/2023 9:46 AM | |
Joined: 4/15/2022 Last visit: 7/31/2024 Posts: 28 Rating: (0) |
Link of that manual is in the first post. Click on the word ”manual”. AttachmentSCLV4_e.pdf (547 Downloads) |
Last edited by: Jen_Moderator at: 04/26/2023 05:28:34PDF attached from link. |
|
Follow us on