7/25/2017 7:54 AM | |
Posts: 10 Rating: (0) |
Dear,
I made correct configuration, added OBs for interruptions (OB40,82,83), checked profibus address and connection few times (DP led on IM is ON) but interface module is "unreachable". I have installed GSD files for IM155-6DP HF firmware v1.1 and v3.1, and I'm using V1.1 because my interface module IM155 has firmware v1.1. Where is possible problem? Do I need to update firmware of IM module to V3.1? Best regards, ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/25/2017 9:28:49 AMNew subject after splitting |
|
7/25/2017 8:18 AM | |
Joined: 5/12/2006 Last visit: 10/22/2024 Posts: 22431 Rating: (3028) |
Hello, how is the LED state of the PLC? Christoph |
7/25/2017 9:11 AM | |
Posts: 10 Rating: (0) |
Dear, Please find attached picture, with commented of each LED status. Best regards, Marco |
Follow us on