6/12/2024 2:15 PM | |
Joined: 7/27/2023 Last visit: 8/30/2024 Posts: 69 Rating: (4) |
Hi! A Basic Panel allows up to 2 files of 10 variables each, which would be the way to store valueson the screen. Here are the specifications: - Scope of functions with WinCC: https://support.industry.siemens.com/cs/us/en/view/90114350/119868383627 And it is configured as follows: - Logging Process Valuesand Alarms with WinCC (TIA Portal): https://support.industry.siemens.com/cs/ww/en/view/109746939 If it were a Comfort HMI you could configure a shared folder on the PC. - Integrating HMI Operator Panels in TCP/IP Networks and access to a NAS or to a shared Windows folder and data exchange via "SIMATIC Option+ Manager": https://support.industry.siemens.com/cs/af/en/view /92346478 |
Last edited by: The Helping Hand at: 06/13/2024 08:04:04Links and text formatting optimized |
|
6/13/2024 4:02 PM | |
Joined: 3/30/2020 Last visit: 8/10/2024 Posts: 21 Rating: (0) |
Hi, The last link is not working. Thanks, Baldeep |
Follow us on