9/19/2006 10:44 AM | |
Posts: 6 Rating: (0) |
Hello, I'm trying to get tip 45b working on an cpu226xm. I build the special hardware and test it with an osilloscoop, all the time's and pulses are correct. It won't read the data on I0.1 in the 13 counts. Will it work on an cpu266xm? Hase anybody this tried? Any help would usefull. Thx. Attachmenttip045b.zip (374 Downloads) |
9/19/2006 11:59 AM | |
Posts: 6 Rating: (0) |
Hello wizzard, We test it with an osilloscoop for the timing and duration of the pulses, acording the osilloscoop everything was oke. What also was confusing, is the picture on the documentation. From the temp. module you see 4 wires to the amplifying circuit, so far I know there are only 3 wires. the pulse, data and the minus. When I monitor the program vw2 go's from 13 to 12 and will reset everything. I tried to set the time intervall on 35 because the cpu216 reads from 5 to xxx and the cpu226 reads from 0 to xxx ms. But it won't work. AttachmentTEMPERATUR-ZEITMODUL.pdf (354 Downloads) |
Last edited by: leob at: 9/19/2006 12:04 PM |
|
9/19/2006 4:50 PM | |
Joined: 4/24/2006 Last visit: 9/17/2024 Posts: 8738 Rating: (1168) |
Hello leob, Just wondering: have you tried to change both inputs? Best regards, Wizard |
9/19/2006 10:55 PM | |
Posts: 6 Rating: (0) |
Hello wizard, I tried to change the wires but vw2 goes to 10 and stops. Regards, leob |
Follow us on