4/8/2008 7:35 PM | |
Posts: 2661 Rating: (279) |
Yes, for V5.0 and greater, it is possible to do a online upgrade. See the following FAQ: Operating System Updates for S7-416-CPUs: http://support.automation.siemens.com/WW/view/en/2858911 |
4/9/2008 6:53 PM | |
Posts: 2661 Rating: (279) |
I also could not locate the procedure in the manual mentioned in the FAQ. But there is online help available (in HW Config)for upgrading the CPU firmware. Please read this online help thoroughly. AttachmentDokument1.pdf (318 Downloads) |
8/19/2008 9:23 PM | |
Posts: 67 Rating: (0) |
So if I have V1.2 the only possible way is to pay for the card and find a programmer to program the card correct? There is no other possible way? |
8/19/2008 10:39 PM | |
Posts: 67 Rating: (0) |
Yes you are correct. Thanks. I missed that section on the page and we ordered the card blank but now our programmer decided it doesn't want to work. |
Follow us on