9/27/2020 10:48 PM | |
Posts: 110 Rating: (0) |
Hi, After spending some time I could not find the address any where but the block FC6 (DP recieve) has been used in another FC to fetch some data (issue happens due to this location i suspect). I found only IW178 which is moving to some DB...am wondering if this is the reason?. Attached the screenshot of program Regards Sandy AttachmentFC6.pdf (364 Downloads) |
9/28/2020 2:05 PM | |
Posts: 110 Rating: (0) |
Hi,, Yes I searched for PQW17 or QW178 in reference editor but could not find it...is there any other way to search this?? Regards Sandy |
9/28/2020 2:08 PM | |
Joined: 4/24/2006 Last visit: 10/18/2024 Posts: 8746 Rating: (1169) |
Hello, When looking in diagnostic buffer, it looks like the problem is in FC6 Best regards, Wizard |
9/28/2020 2:10 PM | |
Posts: 110 Rating: (0) |
Attached the Diag buffer from the system AttachmentDiagnose.txt (315 Downloads) |
9/28/2020 2:47 PM | |
Posts: 110 Rating: (0) |
Hi, FC6 is DP_RECV and it has been called in another FC. Everything is working fine and it was good for years..recently this issue started. now I have found the two CP card which is used for DP communcation and attached the pdf file. but the address 178 is no where mentioned Regards Sandy AttachmentCP card.pdf (369 Downloads) |
9/28/2020 3:16 PM | |
Joined: 4/24/2006 Last visit: 10/18/2024 Posts: 8746 Rating: (1169) |
Hello, In hardware configuration, you find no QW178? Perhaps the DP/DP couplers use it? Best regards, Wizard |
9/28/2020 3:29 PM | |
Posts: 110 Rating: (0) |
Hi, no either in HW config or reference editor QW178 not used also checked the DP coupler.... Regards Sandy |
Follow us on