4/12/2019 4:54 PM | |
Joined: 5/7/2018 Last visit: 6/11/2024 Posts: 7 Rating:
|
Hi everyone, I've been working on a project that consists basically in integrate a conventional chatbot in IOT2040, to make some actions and get some information. This is very common and usefull in a home automation system, buy why don't we use this features in a industrial environment? So here it is ! Im sharing with you an integration between IOT2040, fully programmed with Node-Red, and Telegram. The basic functions are described bellow:
How to do it? First of all, you have to download the Telegram app on your smartphone. After that you must to create your own bot and for that, you have to start a conversation with @botfather and follow the steps described in the link bellow (step 6 more precisely): https://core.telegram.org/bots Once created, you can start with the Node-Red programming. I attached the entire flow that I used in this application, sou you can import to your project. You just have to configure your bot ( name and token ) and start the application. There are some commands and functions,as well as:
All the information are transfered via MQTT, like voltage, current and production. I hope you enjoy this applicantion, please test and let me know how was it ! PS: Your can download the file with some pictures in the link bellow: AttachmentFiles.zip (684 Downloads) |
Last edited by: Vinicius Basilio at: 4/12/2019 8:35:30 PMLast edited by: Jen_Moderator at: 4/15/2019 8:52:55 AMRemoved link and added all files as an attachment. |
|
This contribution was helpful to
5 thankful Users |
Follow us on