3/6/2025 10:24 AM | |
Joined: 4/11/2022 Last visit: 9/14/2025 Posts: 90 Rating:
|
Try the address 8192. |
Rgds, |
|
3/6/2025 10:57 AM | |
Joined: 3/5/2025 Last visit: 3/6/2025 Posts: 4 Rating:
|
Tried - still no comms. Thanks anyway! |
3/6/2025 11:10 AM | |
Joined: 3/5/2025 Last visit: 3/6/2025 Posts: 4 Rating:
|
The part number on the front is 6ED1052-1MD08-OBA2. The firmware is version is 1.84.03 Thanks! |
3/6/2025 12:14 PM | |
Joined: 3/5/2025 Last visit: 3/6/2025 Posts: 4 Rating:
|
Well..... thats annoying. I guess I will look into S7 instead of modbus. |
3/8/2025 12:10 AM | |
Joined: 11/2/2024 Last visit: 3/24/2025 Posts: 14 Rating:
|
You can try ModbusHD, also note that in Modbus TCP, 1 is subtracted from the register address. You can also try some programs that I uploaded to this forum, which are for testing with Modbus TCP using LOGO! as a server. I have also used node-red (node-red-contrib-modbus) with LOGO! and have had no problems. AttachmentModbusHD.zip (279 Downloads) |
Follow us on