9/13/2024 9:02 AM | |
Joined: 5/6/2022 Last visit: 10/14/2024 Posts: 465 Rating: (92) |
Hi sam2014, Responding to your second question, I have been checking and in the delivery release of the PCS7 V9.1 SP2 software, you can see some IPCs compatible with the software and I understand that if the IPC has a released operating system compatible with the software, it is also suitable for use. Here is the link to the delivery release: "Sales and Delivery Release: SIMATIC PCS 7 V9.1 Service Pack 2 EU & ASIA" Best regards!
|
If this Information really helps, you could use the Rate function |
|
9/13/2024 7:29 PM | |
Joined: 7/30/2014 Last visit: 10/14/2024 Posts: 151 Rating: (1) |
Hi ElonksuM_SN_BN Thank you for answering me, i checked the list showing in the link and i didn't find the ipc1047E i am not sure if it's not compatible or just because it's a new product. can you confirm if it is compatible? best regards |
Follow us on