5/3/2024 8:33 AM | |
Joined: 1/21/2013 Last visit: 6/17/2024 Posts: 2888 Rating:
|
Hi Nicolas, Yes, you can use third party motors with SINAMICS S120. The last time I used the S120 I had to control four linear motors. Presumably the motor manufacturer can provide the motor data that you need to configure within the S120. However, you will need to connect the encoder, which may require additional hardware. It does not matter how you control the motor later, but for safety features you will need a safe encoder signal. I would recommend that you contact your local Siemens technical consulting to clarify the details. Kind regards |
Follow us on