8/14/2024 2:46 AM | |
Joined: 4/6/2021 Last visit: 8/14/2024 Posts: 1 Rating: (0) |
I am experiencing the opposite case. I need to download the image version of my TP177 micro HMI to be able to load the .psb file with Prosave. My .psb file is version V01.02 and the PT file is V01.08. What should I do in that case? ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 08/14/2024 08:28:43New subject after splitting |
|
9/5/2024 1:42 PM | |
Joined: 8/3/2009 Last visit: 9/27/2024 Posts: 13803 Rating: (1741)
|
Hello Marlon Rodriguez Image versions are integrated in the corresponidng WinCC flexible version. Here is a good overview: https://support.industry.siemens.com/cs/de/en/view/21742389 But if you have a Backup with Prosave you should be able to restore it into any other OS Version of the same panel. the Backup should include the image version Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on