7/27/2023 6:09 AM | |
Joined: 3/25/2015 Last visit: 7/30/2024 Posts: 63 Rating:
|
Hello I'm having problems with a 4Gb non-Siemens usb stick not being recognized by the HMI KTP700 Basic. The usb stick is working fine on every pc I plugged it in. Even on a TP1900 Comfort. Is there a minimum required size required for KTP700 to be able to recognize it? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/27/2023 11:17:25New subject after splitting Kind regards |
|
7/31/2023 11:17 AM | |
Joined: 8/3/2009 Last visit: 8/7/2024 Posts: 13486 Rating:
|
Hello simonspt No I think there is nothing damaged on your device. We tried also different USB Devices on our Basic Panels 2nd Gen. Only a few worked also in our tests. I have also different sticks that works (2GB, 16 GB...). Here are the specifications for the USB Recovery: https://support.industry.siemens.com/cs/de/en/view/109744950 But the USB Stick from Siemens that is released as accessory is also a 32GB with USB3.0 ... so I´m not 100% sure what are the definitiv criteria for a working one... but Siemens Stick should work bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on