(0)| 11/10/2025 4:07 PM | |
|
Joined: 10/17/2007 Last visit: 1/18/2026 Posts: 4579 Rating:
|
Please post the module picture, I need to see close look of Siemens label on the module BTW, after I search from Google, I remind myself, your module is Siemens MCU172, which is developed in 1996, and I have been trained to set up this module in 1997 in Nuremberg Training center. It is a single axis positioning control--I think it is previous version of SIMODRIVE 611U (which is set up by SIMO COM U), but both of these 2 kinds of module were discontinued, if you want to download MCU172 manual see attach file for the link ATTENTION--the link is not from Siemens (stop for supporting ) you have your own risks to download.
Attachmentold_link.pdf (106 Downloads) |
Last edited by: nulizhang at: 11/10/2025 16:47:24If you like my comments please |
|
Follow us on