4/23/2021 6:13 AM | |
Joined: 8/25/2006 Last visit: 9/9/2025 Posts: 2218 Rating:
|
Hello. Add new IM to Profibus in HWConfig, add required modules to the IM. Configure CRV/CTV for this IM in CFC and virtual connections as discussed earlier. Instead virtual connections you can use pointer-based communication (CRV_P/CTV_P), look at sample project in Simatic Manager 'D7-TDCbasic', D01P01, Chart 'Com_Profibus'. |
This contribution was helpful to
1 thankful Users |
4/23/2021 8:34 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject How to install new AI card in IM153 and its configuration in TDC side? is published within the conference SIMATIC TDC, FM458, T400. Jen_Moderator |
Follow us on