(0)| 2/12/2021 11:41 AM | |
|
Posts: 1 Rating:
|
During start-up we have one motor we can't get started. We get the alarm " Execution ON command". When we give the ON-command over our DCS system we directly get the fault. The main relais even don't get activated. Any idea what could be wrong? Simocode is used for a star/delta starter. BU inputs are used to send the start/stop signal to our DCS and DCS is controlling the motor. In attachment a copy of the project. Regards Attachment376S014 - Test TIA16.zip (812 Downloads) |
Last edited by: matthias.decock at: 02/12/2021 11:42:39 |
|
| 4/15/2025 2:19 AM | |
|
Joined: 2/22/2024 Last visit: 4/15/2025 Posts: 2 Rating:
|
apakah ada jawaban terkait perintah execution on command ? saya juga bingung terkait hal ini |
Follow us on