9/12/2025 2:04 PM | |
Joined: 12/5/2023 Last visit: 9/12/2025 Posts: 12 Rating:
|
Hello, Regarding the 6 points you mentioned, I would like to point out that we could not find where to observe the Batch Trace in point 5, while for the other points, I can say that the system is consistent as you indicated. I have also tried to show that the issue still persists with the short summary below and the attached videos. Our system has 2 Batch Servers running on version V9.1 SP2 UC07. Our main problem is that when both Batch Servers are powered on simultaneously, Batch Server-2 cannot perform its redundant task. As shown in the attached video, DBMon gets stuck at "Processing," and the SBS part remains at "Listening_Prepared." After this hang occurs, restarting Batch Server-2 resolves the issue. You can see this in the attached Video 2. To identify the root cause, we downgraded all system versions to V9.1 SP2 and created a new project. However, we observed the same issue in a slightly different way: both servers get stuck with statuses showing as not Running and DBMons stuck in Processing. We then upgraded the project to V9.1 UC04 and tested with a new project again, but the problem persisted. We have tried many approaches, but the situation remains as shown in the videos. We would greatly appreciate your assistance regarding this issue. Attachmentvideos.zip (14 Downloads) |
Follow us on