(0)| 2/4/2016 6:52 PM | |
|
Posts: 1 Rating:
|
Port 2000 is used to communicate between the IO server and an RNI (i.e. DOS_NIM), IEM, or EIM. Between the IO server and the SCADA/HMI layer, the Suitelink protocol is utilized and uses Port 5413 (tcp) The SuiteLink Service (a.k.a. slssvc.exe) in WonderWare SuiteLink before
2.0 Patch 01, as used in WonderWare InTouch 8.0, allows remote
attackers to cause a denial of service (NULL pointer dereference and
service shutdown) and possibly execute arbitrary code via a large length
value in a Registration packet to TCP port 5413, which causes a memory
allocation failure. -- OR --
|
Follow us on