(1)| 4/2/2008 3:35 PM | |
|
Posts: 467 Rating:
|
Hello, you can configure Simocode pro V as basic type 1 or basic type 2. With basic type 1 you can read 2 bytes binary data and 4 analog values (in word format). At basic type 2 you read 2 bytes binary data and one analog value. You can define this values yourself e.g. via the software Simocode ES. For accessing this values in S7 you can use the commands of the process image, like e.g. A I x.0 L IW xy Usually there is no need to use SFC 14. If you need to read out still more values you have to use SFC59 (reading data records). You find the relevant data records in Simocode manual chapter B. (http://support.automation.siemens.com/WW/view/en/20017780). |
Follow us on