(0)| 11/4/2008 6:50 PM | |
|
Posts: 7 Rating:
|
Tim, I have seenNIM32 stop responding, when using the "Control Simulator" or "Control Engine". Restarting the NIM32 service does notsolve the problem.The only way I have been able to recover is to reboot the PC and then re-start each simulated controller. To address peer to peer communications, you can use the "Control Engine" instead of the "Control Simulator". It is alicensed item,but this is the only way for you to simulate an ACM and communicate, via Mbus or Mnet, to differentI/O servers. The ControlEngine also supportsthe serial ports on the host PC, for MODBUS communications. Reference Doc: CG39CTRLENG-1, Rev: 2, August 2003 The Control Engine is intended for use as a supervisory controller for overseeing control loops that operate independently, but are subject to intermittent corrective action, such as through setpoint adjustment, and is generally used for some degree of coordinating overall production of a plant or process unit.4.2 Control Engine VS. ACM The Control Engine has most functions in common with an embedded hardware-based ACM. Functionality details can be reviewed in the ACM documentation (see section 1.5, “Related Literature”). The Control Engine differs from an ACM in the following areas: ... I/O – The Control Engine is intended for supervisory control, it does not directly connect to physical I/O channels. However, it can directly connect to other control modules [i.e., Advanced Control Module (ACM) and Critical Control Module (CCM)] on the MODULNET (M_NET) or MODULBUS (M_BUS) when Communications functions blocks are used within resource configurations and the host PC is equipped with an M-NET/M-BUS Interface Card. LIL – The Control Engine supports direct serial communications, using the serial port on the host PC, with the Local Instrument Link (LIL) and Modbus control networks and related function block libraries (such as LIL_320 and Modbus). AttachmentCG39CTRLENG.pdf (983 Downloads) |
Last edited by: Electrowiz at: 11/4/2008 7:30 PMUpdated Last edited by: Electrowiz at: 11/4/2008 7:06 PMUpdated |
|
Follow us on