(0)| 12/19/2018 11:27 AM | |
|
Posts: 27 Rating:
|
The absolut adresses are in PC Access (OPC) equivalent to in Smaller scale/Win. Typically you will utilize the representative names (same as in Small scale/Win, as well). Similar to no Windows software engineer, I have just utilized the test customer, which accompanies PC Access (I use CPU224XP and Miniaturized scale/WIN V4.0). PC Access taking care of in detail: - in the tree on the left site tap on Miniaturized scale/Win(..) - r-click > new PLC... - right PLC adress if neccessary and squeeze alright - tap on NewPLC - New >Item and after that characterize a variabl e.g. VB0 and press alright You can do this multiple times for a few factors - squeeze catch "Add Current Thingsto checkCustomer" - squeeze catch "Test Customer Status" - > now you see the qualities in the beneath windows of PC Access I can prescribe to peruse the online help of PC Access particularly the reference part. |
Last edited by: cat1229 at: 12/28/2018 7:51:37 AM |
|
| 5/14/2020 12:38 AM | |
|
Posts: 1 Rating:
|
If you would require to have the knowledge about the working of the PLC, it is essential that first, you have the understanding of its central processing units’ (CPU's) scanning sequence. The methodology would be basically going to be the same for all PLCs. However, as special hardware modules are going to be added into the system, additional scanning cycles would be required. Upon powering-up, the processor would be able to scan the input module as well as transfer the data contents to the input's image register or table. Data from the output image table is going to be transferred to the output module. I have learned all about the PLC, while I was learning for my certification program in here at Spoto Dumps. I must say that their expert trainers have helped me a lot and have cleared all my doubts, which build up confidence in me for appearing for the exam and clear them in a single attempt. |
Last edited by: Jen_Moderator at: 05/14/2020 06:33:21Edited text for better reading. Last edited by: Jen_Moderator at: 05/14/2020 06:36:45Removed advertisement link. Last edited by: AaronKil at: 05/18/2020 23:17:27Last edited by: AaronKil at: 05/19/2020 19:34:42Last edited by: AaronKil at: 05/19/2020 19:35:32Last edited by: AaronKil at: 05/20/2020 16:45:45Last edited by: AaronKil at: 05/21/2020 13:27:00 |
|
Follow us on