3/22/2025 7:29 PM | |
Joined: 9/4/2024 Last visit: 3/26/2025 Posts: 1 Rating:
|
One question: What would be the correct way to map devices? If it's not possible through the ABT Site or via the web, would this necessarily be done with Desigo CC? Do you have a manual for creating BACnet points on the ABT Site? ------------------------------------------------------------------------------------------ |
Last edited by: AutoGen_2536550 at: 03/22/2025 19:30:03Last edited by: Moderator_Lan at: 03/24/2025 08:31:46Text formatting optimized Last edited by: Moderator_Lan at: 03/24/2025 08:32:59New subject after splitting |
|
3/26/2025 3:02 PM | |
Joined: 11/8/2017 Last visit: 8/23/2025 Posts: 355 Rating:
|
Hi, There are a couple of ways to create BACnet points in ABTSite. The easiest way is done when in the 'Engineering' tab of your controller, and then within the 'BACnet References' section. There is some good information in the ABTSite Help files. Refer to the attached screen dumps for the locations. Regards, AttachmentCaptures.zip (228 Downloads) |
Follow us on