9/4/2025 7:26 AM | |
Joined: 8/3/2009 Last visit: 9/10/2025 Posts: 16371 Rating:
|
Hello AutoGen_bb728 for WinCC Runtime Professional you will NOT need additional Licenses for OPC UA Server functionality. (it is different to WinCC V7/8) Also there is no connectivity license or similar for WinCC Professinoal. Here is a good overview which OPC UA Specifications are supported in which Version: https://support.industry.siemens.com/cs/de/en/view/109763315 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on