6/17/2021 9:23 PM | |
Joined: 9/23/2005 Last visit: 9/10/2025 Posts: 4416 Rating:
|
Hi As from TIA V17, it is possible to configure Two-Hand operation features: that means that to operate one object it is necessary that a second object (button) would be pressed at same time. That intends to avoid unintentional operation of a control. Steps to configuration
TIP: this feature could be used just with multi touch monitors / screen. However it is possible to see the effect that the released / pressed enable button generate on the linked devices (grayed or not) even using a mouse. Sample project. AttachmentUni20_20210617_1617.zip (926 Downloads) |
Last edited by: Denilson Pegaia at: 06/17/2021 21:23:43Denilson Pegaia |
|
This contribution was helpful to
2 thankful Users |
Follow us on