(0)| 1/22/2026 4:07 PM | |
|
Joined: 1/22/2026 Last visit: 1/23/2026 Posts: 2 Rating:
|
Hi community, I would like to use a free telegram in S7 for my 6sl3244-0bb12-1fa0. When I choose the cu240e from the S7 hardware list, I can choose the option ‘free telegram’ 17/12. When I download the G120_GSDML_CU240x_PN_V4.7_SP13 file, install it in the hardware from S7, I don't have the option anymore to select the ‘free telegram’ 17/12. I would like to use the gsdml file because I don't want to integrate the starter project in my s7 project. How do I use the gsdml file with a 17/12 telegram function? Thanks in advance, L ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 01/23/2026 07:35:00New subject after splitting |
|
Follow us on